Search   Start

Quick Links


SICK is one of the world’s leading manufacturers of sensors, safety systems and automatic identification products for industrial applications. Whether automating factories or optimizing distribution centers, SICK provides cost-effective solutions.

SICK has been a technology leader for more than 60 years. Leveraging a history of innovation, the company has pioneered a long line of industry firsts – such as the first safety light curtain, the first color sensor, and many more. These innovations provide solutions to the automotive, airline, manufacturing, packaging, and material handling industries.

The North American subsidiary of SICK was established in 1976. Company headquarters are located in Minneapolis, Minnesota, with sales throughout the U.S., Canada, and Mexico. SICK employs more than 4700 people worldwide, with 2007 sales at nearly €708 million.
Contact
SICK
6900 W 110th St
Minneapolis, MN
55438 USA

Phone:
800.325.7425
Email:
info@sick.com
New Products from SICK 
With high resolution and fast switching speeds, the HLG augments the versatile array of existing light grid solutions from SICK. Ideal applications for the HLG include part counting and leading edge detection on a conveyor.

Learn more about the HLG.


The compact BKS/PKS/XKS Encoders are easy to install and use and are ideal for the most complex linear positioning applications. These encoders also have a different mechanical design than our other wire draw encoders, enabling them to be directly mounted to the wire draw mechanism, eliminating additional accuracy deviations from a shaft coupling.

Find out more about these new encoders.
The C4000 Select Safety Light Curtain helps reduce downtime because it can be configured quickly, using DIP switches right on the device – rather than a PC. It is also easy to install and align with an integrated laser alignment bar graph system… and condensed, intuitive diagnostics make troubleshooting simple.

Find out more about this unique, new safety light curtain.
The DS30 combines simple push button setup with incredible detection performance – all in an industry standard housing. What makes the DS30 unique is its ability to detect flat black and shiny targets at the same range repeatedly.

Click here to learn about the features and benefits of the DS30.
top of page