Search   Start

Quick Links


SICK is one of the world’s leading manufacturers of sensors, safety systems and automatic identification products for industrial applications. Whether automating factories or optimizing distribution centers, SICK provides cost-effective solutions.

SICK has been a technology leader for more than 60 years. Leveraging a history of innovation, the company has pioneered a long line of industry firsts – such as the first safety light curtain, the first color sensor, and many more. These innovations provide solutions to the automotive, airline, manufacturing, packaging, and material handling industries.

The North American subsidiary of SICK was established in 1976. Company headquarters are located in Minneapolis, Minnesota, with sales throughout the U.S., Canada, and Mexico. SICK employs more than 5000 people worldwide, with 2007 sales at nearly €708 million.
Contact
SICK
6900 W 110th St
Minneapolis, MN
55438 USA

Phone:
800.325.7425
Email:
info@sick.com
New Products from SICK 
The OD Precision Sensors are the only optical displacement sensors on the market to connect three sensors to one controller, making it easier to consistently measure the x-, y- and z-axes. The OD Precision is simple to set up and requires less hardware than similar solutions… …

Click here to learn more...

The IMF, MH15V and V18V are all field tested to perform to customers’ real needs. These sensors are IP 69K-rated, ideal for the food and beverage industry. They also augment the wide range of wash down-rated solutions from SICK, including a full range of IP 69K sensors, sensor cables, junction boxes, and enclosures for safety solutions and bar code scanners.

Click here to find out more.
Speed, power, flexibility and ease of use are the features that define the new CLV620 and CLV630 Laser Bar Code family. They are ideal for a wide range of automation applications, such as retail distribution, high-speed packaging and document handling.

Click here to learn more…
The UC4 is the smallest ultrasonic sensor from SICK. It offers excellent detection of optically difficult targets, such as clear materials and provides perfect performance in optically challenging environments.

Find out more about the new UC4.


top of page