Skip Navigation Linkssick.com > EN > Home > Solutions > Industries > traffic
Print

Traffic 
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
The transport of goods and the movement of people is today optimized to a large degree using control and safety systems. Sensors for measuring and recording different types of data form a substantial basis for a robust and long-lasting performance of such systems. To mention but a few examples: Laser measurement systems classify vehicles as part of the road toll system, automation light grids reliably detect people at train door systems and dust measuring devices and gas analyzers measure pollutant concentrations in tunnel areas. This is where you can fall back on the long standing experience of SICK sensor technology in the outdoors area. An extremely wide range of robust and innovative products in transportation systems, combined with a worldwide service and sales structure have made SICK a market and technology leader in many fields of the traffic and environmental data acquisition. Here are a few application scenario
Click to show / hide content block    Web Part Container
Click to show / hide content block    Content Block 02
Show Content 
No Links 
Hide Title 
Show Subtitle 
Show Image 
 

 

Toll stations 

 
 
At toll stations in each single lane, the vehicle classification has to be determined exactly and very quickly both in manual and in "free flow" operation. Moreover, the positions of the vehicle front and end have to be sent to the control system for the barriers such that these open and close quickly enough, but not too quickly. This alone ensures that the vehicle is not damaged and that fraud cannot take place.  SICK offers dedicated systems to this end, either on the basis of distance measuring multi-beam laser scanners or based upon measuring light grids. While the high-precision laser scanners are suitable for overhead mounting and thus reduce maintenance costs considerably (no contamination), the robust and extremely sunlight-resistant SICK light grid solutions can be integrated in existing structures and classification systems very easily.
Click to show / hide content block    Content Block 03
Show Content 
No Links 
Hide Title 
Show Subtitle 
Show Image 
 

  

Road toll system on highways  

 
 
In many countries today, "Multi-Lane Free Flow" (MLFF) systems are used as a nationwide road toll and monitoring system. SICK distance measuring multi-beam laser scanners are excellently suited for the high-precision classification of vehicles in overhead mounting – even then when the vehicles change lanes. Mounting above the roadway allows easy access and greatly reduces the costs for maintenance and deployment in comparison to sensors on the ground.
Click to show / hide content block    Content Block 04
Show Content 
No Links 
Hide Title 
Show Subtitle 
Show Image 
 

 

Sensors for tunnel ventilation   

 
 

Road tunnels have to be supplied with sufficient fresh air during operation. Depending on the fleet segmentation (percentage of trucks/cars, diesel fuled engines, pollutant classes, etc.) and various other secondary conditions, different lead components for controlling the supply of fresh air can arise. Today, for example, the CO concentration is not anymore the lead component for ventilation control (except in tunnels in very high-altitude mountainous terrain). During the last decade visibility has taken over this role and nowadays NO2 (not NO, due to the strongly fluctuating proportion of primary NO2s) becomes increasingly more significant and is already the lead component for ventilation control in many modern tunnels.
The complete range of products from SICK for measuring devices that are developed and built for the dedicated use in tunnels embraces the measurement of all gas components typically measured in tunnels and corresponding measurement principles and emphasizes SICK's leadership in both the technology and market in this field.

Click to show / hide content block    Content Block 05
Show Content 
No Links 
Hide Title 
Show Subtitle 
Show Image 
 

 

Smoke detection in tunnels   

 
 

Tunnel fires rank among the most fearsome occurrences in road and rail traffic. In more and more studies, something has been substantiated that experts have known about or had an inkling of for a long time – namely, that the optical measurement of smoke density is the quickest and generally most reliable way to detect fires early. Only approx. 10 to 15 minutes are available for self-rescue in the event a vehicle fire has not been extinguished. Along with the quick detection of a fire – e.g. with a SICK optical smoke detector – it is also very important that the distribution of smoke is recognized and to ensure best possible stratification of smoke on the tunnel ceiling. To this end, it is essential that for exact information on the flow velocity, measurements are taken over the entire width of the tunnel (e.g. with FLOWSIC200) and not only at a single point.

Click to show / hide content block    Content Block 06
Show Content 
No Links 
Hide Title 
Show Subtitle 
Show Image 
 

  

Projection and overheight checking 

 
 
Vehicles of excess height can cause severe damage to civil engineering structures such as tunnel mouths and bridges and thus bring about unnecessarily long blockage periods. Products from SICK, such as the HISIC450 or LMS111 detect reliably and without contact vehicles of excess height such that appropriate countermeasures can be introduced in time. The photoelectric sensors used in HISIC450 are distinguished by a robust design and by plenty of reserve light, the LMS111 can also be used to detect the position (lane) of a vehicle of excess height.
Click to show / hide content block    Content Block 07
Show Content 
No Links 
Hide Title 
Show Subtitle 
Hide Image 
 

 

Speed and red light monitoring   

 
 
The practical use of speed and red light monitoring systems considerably increases safety in the road traffic network, and the number of accidents and even road deaths are lowered demonstrably. SICK laser measurement technology provides here highly accurate measurement results that, to a great extent, are not manipulable.
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
Find our Products & Solutions

Sensing solutions for transportation systems

safetyPLUS
safetyPLUS – competence in safe machinery
Know-how, system integration, standards and regulations, FAQs ...

Other solutions

Button to start the search