Skip Navigation Linkssick.com > EN > Home > Solutions > Industries > Tier Ones
Print

Part Supplier - Tier Ones 

 
Click to show / hide content block    Page Header
Hide Page Header 
Hide Date 
Hide Subtitle 
Hide Leadtext 

Tier Ones 

   
Click to show / hide content block    Content Block 01
Show Content Element 
No Links 
Show Title 
Hide Subtitle 
Show Image 
 

SICK provides more than sensor technology solutions to all sectors of automotive parts production 

 

 
 
Discover step by step how SICK “Sensor Intelligence” makes processes in and around your automotive parts production faster, more efficient and safer. Based on selected applications that we have illustrated as examples, we will highlight the wide range of options provided by our intelligent sensor solutions. See for yourself and discover your potential for optimization.
We will of course assist you.
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
Seats 

 

 
 
Prior to delivery the adjustments on the seats are checked. An IQ80 inductive proximity sensor signals the presence of a carrier and stops the transport. Two DME5000 distance sensors measure the seat adjustments to be checked. For this purpose the worker pushes the seat to its front and rear position and reads the two measured values directly on the display on the bottom DME5000.
Click to show / hide content block    Content Block 03
Show Content 
No Links 
Show Title 
Show Subtitle 
Show Image 
 

Mechanical Parts  

Motors 

 
 
The ICR840 code reader reads the two-dimensional code applied by a laser (direct part marking) to a camshaft and checks whether the correct camshaft is fitted. The device sends the information to a central computer for quality assurance.
Click to show / hide content block    Content Block 04
Show Content 
No Links 
Show Title 
Hide Subtitle 
Show Image 
 

Tires 

 

 
 

Tire identification using the OPS890 bar code reading system. The system comprises eight CLV490 line scanners arranged to reliably detect the bar code on the tire bead. The reading system is triggered by two WL18 (A) photoelectric reflex sensors that are arranged in an X-shape in the reading zone to reliably detect the tire. Two further WL18 (B) photoelectric reflex sensors arranged one over the other provide fast pre-adjustment of the position of the focus of the code reader.
The large depth of field of the devices does not require any further adjustment.

Click to show / hide content block    Content Block 05
Show Content 
No Links 
Show Title 
Hide Subtitle 
Show Image 
 

Assembly of small parts 

 

 
 

A handling robot fits two sealing rings to injection nozzles. It picks up the injection nozzle from the conveyor belt and places it in the receptacle on the assembly table (process not shown here). A WT12L laser photoelectric proximity sensor monitors for presence in the receptacle and the exact positioning of the nozzles. The rings are supplied on two vibration conveyors. WF fork sensors mounted at the outlet on the conveyors control the vibration conveyors such that rings are always available. IQ05 inductive proximity sensors check the presence of rings in the two pick-up stations. The handling robot collects a ring using end effectors attached to its pivoting arm and fits it to the nozzle. The end effectors are actuated using pneumatic cylinders. MZT6 magnetic cylinder sensors poll the position of the piston in the cylinder. Once both rings are fitted, the robot replaces the nozzle on the conveyor belt where an ICR840 code reader reads the two-dimensional code applied by laser (direct part marking) and transmits the information to a central computer for quality assurance.

Click to show / hide content block    Content Block 06
Show Content 
No Links 
Show Title 
Show Subtitle 
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
Find our products and solutions

Other solutions

Button to start the search