Skip Navigation Linkssick.com > EN > Home > Solutions > Industries > Building Automation
Print

Building Automation 
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
Comprehensive building automation with tailor-made sensor solutions 

 

 
 

Bridge up any security gaps before they appear.
The business field Building Automation has the task to fulfill the customer needs of security, protection and control for buildings and facilities.
We can offer you a wide range of effective options for managing and protecting your property. In building automation, the global perspective counts, which is why SICK is represented all over the world. As an independent partner, we will accompany you at all times and be quickly to hand. The sooner you involve us in your planning, the more effectively our consultation will aid your planning and implementation of certified and high-performance solutions.
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
Perimeters/Fences/Walls 

 

 
 

For building automation of a perimeter, fence or wall, we distinguish two application areas area monitoring and location indicator systems.
With area monitoring, software in the sensor will manage all monitoring areas. The system signals if intruders are present by releasing the switching output and triggering an alarm whenever an area is violated. This may, for instance, also be triggered by objects or items regardless of whether they are mobile or not.
The sensor uses the measuring data with which it has been provided to determine the location.
When this is done, the devices are set so that small animals, adverse weather conditions or mere passers-by do not trigger any false alarms. Another important feature is that the devices take privacy into account. Unlike other protective devices, SICK sensors only record contours for personal identification and not real images. This means that the system will be able to tell that somebody is present within the monitored area but not who it is.

Laser Scanners

  • Makes undetected intrusion into an area extremely difficult
  • Detects events at the perimeter of an area
  • Fence protection, protection of approach areas
  • Protection and/or monitoring of entrances
  • Excavation protection (with horizontal/diagonal setup)
  • Large monitoring areas
  • Storage of all kinds of surrounding contours as references
  • Not impaired by surrounding lighting
  • Fixed-position obstacles can be blanked (e. g. wall constructions)

Recommended products
Laser Scanners: LMS111 LMS2xx outdoor | LD-MRS | LD-LRS outdoor

 

Click to show / hide content block    Content Block 03
Show Content 
No Links 
Show Title 
Hide Subtitle 
Show Image 
 

Open spaces 

 

 
 

SICK laser scanners are usually used horizontally for the monitoring of open spaces. If necessary, several reporting levels can be defined for each scanner (standard function). Approach roads and access paths can also be suppressed so that disruptions to pedestrians or road traffic are prevented. As a result, separate, differentiable alarm notifications are generated. Disruptions due to adverse environmental conditions are intercepted first by the scanner ensuring a low rate of false alarms.
Using these separately output signals, the selected area can be monitored and available cameras controlled via a monitor. This has the benefit that monitor images are displayed according to the incident, considerably reducing the onus on security guards. Further benefits include the shape of areas being user-definable and simple installation on buildings.

Laser Scanners

  • Real-time monitoring up to 360°
  • Precise demarcation possible
  • Insensitive to interference from movements outside of the monitoring area
  • Blanking of certain areas possible
  • Simple adjustment to changes in monitoring conditions
  • Shape of monitoring areas can be defined by user as required
  • Coverage of large areas
  • Separate alarm signals and camera control
  • Can also be installed on buildings with adjacent monitoring areas

Recommended products
Laser Scanners: LMS111 LMS2xx outdoor LD-LRS outdoor

 

Click to show / hide content block    Content Block 04
Show Content 
No Links 
Show Title 
Hide Subtitle 
Show Image 
 

Facades 

 

 
 

Laser scanners are usually used vertically for the monitoring of facades. The size of the monitoring areas and the possibility of setting several scenarios (see example of night/day mode) means only a few systems will be required, making protection as effective as it is inexpensive.
The building's floor outline or fence serves as the reference contour. This is constantly inspected by the system to see it remains intact (distance measurement). Deviations in this outline, e. g. due to movements of earth (excavation) in the monitoring area or manipulation of the laser scanner (dismantling) trigger an alarm. The scanners are highly resistant to environmental influences like rain and snow, making the rate of false alarms very low, something which has also been confirmed by TÜV Süd. 

Laser scanners

  • Large monitoring area
  • As many surrounding contours as desired can be stored as references
  • Prevents excavation
  • No impairments from surrounding lighting
  • Fixed-position obstacles can be blanked (e. g. wall constructions)

V200 Vision System

  • Sender and receiver in a single device
  • Spatial monitoring of tapered areas by fitting a reflector strip or monitoring of straight areas

Light grid

  • Easy integration into window frames
  • Virtually invisible due to flat construction

Recommended products
Laser Scanners: LMS111 LMS2xx outdoor
Vision systems: V200 Work Station Extended
Light Grids: MLG | SGS

 

Click to show / hide content block    Content Block 05
Show Content 
No Links 
Show Title 
Hide Subtitle 
Show Image 
 

Roof Protection 

 

 
 

With flat roof protection, SICK laser scanners are generally installed directly on the building. This removes the need for expensive installations or attachments on the roof. The monitoring area for the system is set up approx. 30 cm above the ground so that any persons crawling under the alarm zone are detected and registered. The edge of the monitoring area can also be placed slightly above the edge of the roof so that any ladders, for instance, are detected at once. The arrangement of the monitored areas, the choice of object size to be detected and flexibly adjustable response times mean any movement of animals, birds or leaves through the monitored area will not trigger an alarm (filter function).

 

Laser Scanners

  • High level of protection against intrusion
  • Seamless monitoring of light domes and bands of light
  • Early indication of break-in attempts
  • Monitoring of large areas using just a few sensors
  • Simple, low cost retrofitting
  • Low installation and wiring costs
  • Prevention of destruction to property with associated low follow-up costs

Recommended products
Laser Scanners: LMS111 LMS2xx outdoor LD-LRS outdoor

 

Click to show / hide content block    Content Block 06
Show Content 
No Links 
Show Title 
Hide Subtitle 
Show Image 
 

Access control and door/gate monitoring 

 

 
 

Areas such as gates and turnstiles can be monitored either using active-switching sensors or a sensor system, which recognizes a special code and then reliably provides access. To do this, either tried and tested bar code reading technology or newer technologies such as RFID with the ISO 14443 standard (special encryption) are available.
Active-switching 2D and 3D sensors and photoelectric sensors, light grids, laser scanners and camera systems (see below) provide a range of options for access detection. The sensor system can be set either so that it recognizes whether an unauthorized person is trying to enter or else how many persons enter a room in order to control parallel systems such as heating, air conditioning or ventilation. 

 

Laser scanners

  • Easy installation (sender/receiver in single housing)
  • Precise location can be detected even for several objects
  • Correct setup can prevent shadowing for the most part

Code reader

  • Robust technology
  • Low follow-up costs for access tickets

Light grid

  • Low-cost system
  • Short response times, fast and reliable detection to prevent reaching in or access

Photoelectric sensors

  • Easy mounting
  • Robust, very low-cost


Recommended products
Laser Scanners: S100 LMS111 | LMS12x 
Code readers: ICR80x | CLV50x
Light grids: MLG ELG
Photoelectric sensors

 

Click to show / hide content block    Content Block 07
Show Content 
No Links 
Show Title 
Hide Subtitle 
Show Image 
 

Indoor areas 

 

 
 

Paintings and sculptures need to be protected from deliberate or accidental vandalism and against theft. Unintentional contact in particular is a challenge for a sensor system as this must be reported without the artistic enjoyment of curators, art lovers or other guests being diminished. The more inconspicuous, precise and reliable protection is, the more this requirement can be met without detriment to the protection. Laser scanners are often used for protection of pictures/walls (vertical) or to protect ceilings/floors (horizontal). For objects such as sculptures, jewelry etc. in wall recesses, light grids have proven to be most appropriate. Fast detection of any interference prevents any “angling” of the object being monitored. Two-dimensional protection is sufficient for paintings but with sculptures, a greater dimensional range needs to be covered. A distance-measuring vision system can also be used for this purpose. 

Laser scanners

  • Certified systems
  • Simple, almost invisible installation
  • Actuators (e.g. a signal system) can be connected directly at exits

Vision sensors/vision systems

  • All-round 3D protection
  • Adjustment to various monitoring objects

Light grid

  • Extra rapid detection of interference in near range
  • Detection of very small objects possible

Recommended products
Laser scanners: LMS12x | LMS100
Vision sensors: V200
Light grids: SGS
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
Find our Products & Solutions

Button to start the search