|
|
|
|
|

Page Header
|
At a glance/Fields of application
At a glance
:
- Software for systematic and efficient CE marking
- Integrated module: StandardManager
- Automatic update algorithms
- Network compatible; data interface to SISTEMA
- Creation of customized libraries
- Modular project building
- Intuitive operating design
Fields of application
- CE-conformance checks on machines
- Risk assessment
- Testing, inspection, and acceptance of machines
- Searching and management of standards and directives
- Creation of technical documentation in accordance with the Machinery Directive
Your benefits
CE marking is an integral part of the design process
Higher effectiveness through early identification of potential weak points
Enhanced competitiveness through avoidance of overdimensioning
Liability risks are reduced
Greater reliability in a maze of standards
Rapid and easy-to-follow project work – simultaneous also possible
Most important new features in version 8.0
User-friendliness
- The user guide has been completely reworked
- Multiple projects can be opened in multiple windows at the same time
- Photos can be linked or embedded at various locations (e.g. in risk assessment)
Safexpert® project manager
- All activities of the CE guide are displayed directly in the project manager
- The newly developed Safexpert® Reminder now also sends a reminder if Safexpert® has not been started
Structuring system projects
- System projects can still be clearly structured from subprojects and modules
- Between the subprojects or modules, interfaces can be defined for which a separate risk assessment is made
Risk assessment
- Measures can be linked to each other
- Cross-reference lists can now be maintained and updated independently
- The risk assessment can be structured and shown according to cross references
StandardManager
- The StandardManager can now always remain open
- Standards being used can be directly applied to the project via drag and drop
- Documents in full text (e.g. standards) can now be stored directly in the database. In this way, Safexpert® can now be operated as a pure client-server application on the company network
Reports, printouts, and exports
- Completely new report generator with individual adaptation possibilities
Check and acceptance assistant (CAA)
- Completely new development with adapted user interface
Client update
- In addition to Silent Installations, Safexpert® is now automatically installed on clients if a newer version is available on the server
Databases
- SQL database with VistaDB
- All data are saved in the SQL database
- Safexpert® manages all data in Unicode
|
|