In addition, users benefit from a high degree of flexibility when choosing the electric interfaces: analog, SSI, Profibus, CANopen, DeviceNet, and HIPERFACE (in future, EtherCAT and Profinet as well) leave hardly anything to be desired in terms of integration.
Measurement requirements and the setting are decisive
Wire draw encoders from SICK are available in a complete range for measuring lengths of up to 50 m. However, the operating environment decides whether an EcoLine encoder, the compact family, or a HighLine device constitutes the best solution. To give an example: For a required measuring length of 5 m, in principle all of the production series may qualify. If a user attaches great importance to the smallest possible construction size, fast start-up via teach-in, and top cost effectiveness, the EcoLine encoders are first choice. On top of that, they offer a version with analog output of measured values – ideal, e.g., for automated guided vehicles. If the setting becomes harsher and all components – i.e. encoders as well – need to be integrated completely into a rugged aluminum housing to prevent any damage, using the wire draw encoders of the compact series is the best option. Solutions involving the HighLine series are proving their worth in any place calling for heavy-duty suitability. Special brush attachments and pulleys ensure that dust, dirt, and moisture cannot penetrate the interior of the rugged housing. Beyond that, the HighLine devices not only offer particularly top-rate shock and vibration resistance – they are also the solution for any types of use that necessitate handling measuring lengths of up to 50 m with a high degree of precision.
Great variety of encoders – for distance measuring made to measure
Not only in terms of application and automation technology, the wire draw encoders of the three series deliver ideal possibilities due to options for integrating different encoder and motor feedback systems; in conjunction with the large selection of communications interfaces, the wire draw encoders from SICK ensure that a made-to-measure solution is available for any type of distance measurement.