Skip Navigation Linkssick.com > EN > Home > Public Relations > Press releases
Print

FlexiLink: Networking a safe control system reliably - For flexible machine designs and interlinked plants 

 
Click to show / hide content block    Page Header
Show Page Header 
Show Date 
Hide Subtitle 
Show Leadtext 

2010-04-26 

Waldkirch, April 2010   
One thing emerges particularly in practical operation of modular plant designs: FlexiSoft safety controllers rarely come singly. And since this is the case, SICK developed a solution toward networking controllers: FlexiLink.
Click to show / hide content block    Content Block 01
Show Content Element 
No Links 
Hide Title 
Hide Subtitle 
Hide Image 
 

 

 

 
 

FlexiLink maps the modular construction of machines consistently. Frequently, various machine modules are only assembled at the user’s location, or they are supplemented there later after operating for a while. In this context, the safety design plays a decisive role, as protection of both the individual module and of the entire equipment constellation must be taken into consideration. This is where FlexiLink comes in. Detection and parameterization of plant components not yet in place but already prefabricated permit implementing this strategy. By way of detecting and parameterizing on site, it is possible to assemble or supplement subsequent machine or plant components without starting up the machine anew.

Intuitive extension of safe control structures

FlexiLink from SICK is a new functionality of FlexiSoft that allows linking up to four FlexiSoft safety controllers with one another in a flexible and functional way.

Integration takes place via a safe device interface from SICK called EFI (Enhanced Function Interface). It serves the connected or, respectively, networked devices to exchange their safety-relevant signals directly – i.e. without additional module. Within the integrated FlexiLink system, the stations can transmit up to 52 bit each.

Setting up a safe FlexiSoft network with FlexiLink is easy. Adding new stations including definition of default process imagers for optional stations as well as administration and diagnosis of the entire integrated system takes place by means of the familiar FlexiSoft-Designer parameterization tool. Thus, the user is familiar with the operator interface and its look & feel. If required, the whole FlexiLink network can be integrated into all of the common Fieldbus systems using the appropriate FlexiSoft Gateways.

For modular, expandable, and interlinked plants

FlexiLink permits integration of FlexiSoft safety controllers into a network wherever plants are designed in a way capable of migration and machine modules interact or are interlinked with one another. Intralogistical facilities and packaging lines are only two examples of application fields in which machine builders and end users can benefit from the advantages of safety- and operation-related networking with FlexiLink.

 

Click to show / hide content block    Web Part Container
Click to show / hide content block  Content Block 02