Skip Navigation Linkssick.com > EN > Home > Public Relations > Press releases
Print

ColorRanger E – High-speed 3D and RGB color imaging  in one camera 

 
Click to show / hide content block    Page Header
Show Page Header 
Show Date 
Hide Subtitle 
Show Leadtext 

2010-03-31 

Waldkirch, März 2010    
SICK is introducing the world’s first high-speed 3D camera with high-quality color capability. By measuring both the 3D shape and the color of objects and parts, more reliable decisions can be made to allow production plants to improve their up-time, through-put, and product quality. The ColorRanger E replaces the need for several different cameras for the same task, which reduces the solution cost and complexity.
Click to show / hide content block    Content Block 01
Show Content Element 
No Links 
Hide Title 
Hide Subtitle 
Hide Image 
 

 

 

 
 

ColorRanger E is the newest member of SICK’s 3D camera product line. The cameras are used as a key vision component by manufacturers and vision integrators worldwide. They solve various inspection tasks by measuring shape, contrast, and surface defects, to ensure product quality and production reliability. The ColorRanger E expands the inspection possibilities further by also providing high-resolution RGB color at up to 3072 pixels per channel. With simultaneous 3D and color information at more than 11 kHz, multiple inspections can be performed in parallel at full production speed.

Improved production quality using both 3D shape and color
3D imaging is ideal where height, shape, or volume is of importance for the production process.  However, to make a complete quality or grading decision, it is often necessary to also consider the color of the parts produced.  This is, for instance, common in grading fruits and vegetables, shape and baking degree verification of baked goods, board grading in the wood industry, quality assurance of electronic assemblies, and fill level and color verification in the cosmetics and pharmaceutical industries. By considering both 3D and color, more reliable inspections can be performed which improves product quality and reduces waste.


Reduced solution cost and system size
ColorRanger combines the functionality of a 3D camera and a line-scan color camera. With SICK’s proprietary MultiScan technology, the camera can be configured to provide several measurements at the same time, such as 3D shape, laser scatter, color, and monochrome, according to the exact need of each specific application. As a result, one ColorRanger can replace several other cameras, which reduces the system size as well as the cost for hardware, integration, and maintenance. In addition, since the different measurements come from the same camera system, it is easier to combine data for analysis.

Superb color quality
ColorRanger delivers high-quality 3D and multi-linear color data, including RGB, near IR, and monochrome without IR content, on a Gigabit Ethernet communication interface. It has a separate row of pixels for each color, which give full color resolution at up to 3072 pixels per channel. The color quality is ensured by well separated color filters of high spectral response, on-chip white balancing, and spatially corrected color channels output. In addition, to eliminate interference from different light sources used for 3D and color imaging, there is a filter option for light source separation.

About Ranger
ColorRanger E is the newest member of SICK’s Ranger product line, which now spans from the low-cost Ranger D for mid -speed 3D applications, to the high-speed Ranger E with MultiScan technology, up to the new ColorRanger E that provides simultaneous 3D and high-resolution color measurements. With their measurement speed, data quality, and high flexibility with MultiScan technology, they can be used in tough industrial environments for various solutions from small-sized component inspection up to large-scale log scanning. The 3D technology is based on laser triangulation using a separate laser source. With this, the user has the full flexibility to adapt field-of-view, height range, and height resolution according the needed of a particular application. With SICK’s easy in-machine 3D calibration tool, the 3D measurements can still be provided in millimeters.
More information at: www.sick.com/ColorRanger

 

Click to show / hide content block    Web Part Container
Click to show / hide content block  Content Block 02