Skip Navigation Linkssick-pa.com > EN > Home > Solutions > Industries > Chemical > Fertilizer
Print

Fertilizer 
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
Fertilizer 
 
Fertilizers are still major products of the chemical industry worldwide. Basically fertilizers consist of nitrates and phosphates. Nitrates are made of nitric acid and ammonia. Phosphates are produced by decomposition of phosphate minerals with sulfuric acid. The basic products for the production of fertilizers are:
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
Production of Ammonia 

 

 
 

Ammonia is produced by a catalytical reaction according to the Haber-Bosch process. Basic materials are nitrogen and hydrogen. The NH3 emissions of the production facilities are continuously monitored. Our solution: 

Click to show / hide content block    Content Block 03
Show Content 
No Links 
Show Title 
Hide Subtitle 
Hide Image 
 

Production of Nitric Acid 

 

 
 

Emission monitoring plays an important role in  the production process of nitric acid. Whereas components such as NO and NO2 were monitored in the past, the focus now has been shifted to the reduction of greenhouse gases and monitoring of N2O. Our solution:

  • Analyzing systems MKAS with analyzer GMS800 with module DEFOR
Click to show / hide content block    Content Block 04
Show Content 
No Links 
Show Title 
Hide Subtitle 
Hide Image 
 

Production of Sulfuric Acid according to the Contact Process  

 

 
 
Sulfuric acid is one of the most important basic chemicals. During production according to the contact process SO2 is catalytically converted to SO3. The SO2 concentration in the process is in the higher vol% range. Its continuous monitoring is made photometrically with GMS800 at room temperature or with MCS300P at higher temperatures. The emission of the process can be monitored with SICK measuring technology. Our solution:
  • SO2-measurement: NDIR analyzer GMS800 or analyzer MCS300P
  • Emission monitoring: Analyzing systems MKAS
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
SICK MAIHAK GmbH
Nimburger Strasse 11
79276 Reute
Germany
Button to start the search